如图中电路,采用的RJ45加网络变压器加TPS2376H供电,但是插入网线后VDD端的输出电压为5V,VSS引脚为-45V,RTN引脚接地,电路无电流输出。后将RILIM由1M改为330K后,电路能输出电流但输出到DC上的电压还是只有5V。将RILIM由330K改为10K后VDD输出电压在5V-50V之间跳变,且网络变压器出现较大的电流声,求问此芯片为什么会出现这种问题,是不是还有匹配电阻或者电容没设置正确。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如图中电路,采用的RJ45加网络变压器加TPS2376H供电,但是插入网线后VDD端的输出电压为5V,VSS引脚为-45V,RTN引脚接地,电路无电流输出。后将RILIM由1M改为330K后,电路能输出电流但输出到DC上的电压还是只有5V。将RILIM由330K改为10K后VDD输出电压在5V-50V之间跳变,且网络变压器出现较大的电流声,求问此芯片为什么会出现这种问题,是不是还有匹配电阻或者电容没设置正确。