This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

为什么TPS65400的基准电压不是0.8V?



原理图参考手册,没有使用I2C,默认Vref应该是0.8V,而实测在0.85V左右,导致输出电压偏高。

搜到之前的相关帖子

e2echina.ti.com/.../226078

但是并没有明确回复。

Vref应该是内部基准电压输出,偏差按手册应该在1%以下,而实际已经达到6%以上。这和什么有关呢?

怎么解决?

谢谢!