目前有个项目,设计要求如下:
输入电压:1-3V
输出电压:3.8V
输出峰值电流:2.3A(峰值电流表现为脉冲形式,持续时间约500us,12%左右的占空比)
输出平均电流:200mA
我在TI网站上找了一圈,发现也就TPS61021A这个芯片比较接近了,现在的问题有两个:
1.规格书上说TPS61021输出3.3V时电流为1.5A,我不清楚是否能够承载2.3A的的峰值电流?
2.规格书上建议输出电容最大为200UF,我如果将电容加大到500UF左右,是否会有问题?
谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好:
上述计算中的3A是规格书上的Valley current limit这个电流吧?
我看规格书的框图上Valley current是过了MOS管之后的,那应该是等于输出电流吧。
3A是输出电流也是平均电流,不是Valley current limit
Valley current limit是指电感电流的谷值