This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76940从SHIP MODE到NORMAL不能正常恢复

Other Parts Discussed in Thread: BQ76940

Hi all,

       

我在使用BQ76940的过程中,现在遇到一个现象,在Normal mode下能正常工作,可是进入ship mode模式后,我给TS1了一个>1V的高脉冲信号,REGOUT也从0V变成了3.3V,但是电池电压采集不正常,

V1~V5可以正常读取,V6~V15,读取全部是0,而且读取的总电压正好是V1~V5的电压之和。三路温度,也是只有第1个温度正确,另外两个也都是0。

请问这是什么原因造成的,我在Normal模式下就能正常工作,从SHIP MODE恢复到NORMAL就有问题。