This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76PL455A 寄存器配置issue



有几个PL455寄存器配置的问题请教下:

1, 如何禁止PL455的UV_FAULT/OV_FAULT,AUXUV_FAULT/AUXOV_FAULT,CMPUV_FAULT/CMPOV_FAULT的检测?

      我们一片PL455可能采集多箱电池组,即跨箱,所以存在某一路/多路采集需要跟上一路并在一起,导致其采集的电压为<=0。

      由于这个原因,想禁止上面提到的这些故障的检测。

      从手册上看,找到了寄存器0x6E-6F,用于屏蔽故障输出。

      从手册上看,UV/OV等这些故障应该会对均衡、开路检测有影响,希望能够关闭这些故障检测功能,而不仅仅是屏蔽其输出。

      我还没有找到如何关闭这些功能的寄存器?

 

2,如何查询开路检测结果?

     查看寄存器0x13,通过设置BAL_CONTINUE可以忽略故障,来进行均衡/开路检测;寄存器0x14-15来进行均衡/开路检测的控制。

     但是没有查找到查询开路检测结果的寄存器?

 

PS:关于第一个问题,希望理想的情况是能屏蔽指定某几路VSENSE的UV/OV故障检测。查看手册寄存器定义,应该是不能实现。

        跟你们确认下,能有办法实现吗?