This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62170过流问题咨询



 你好,目前针对TPS6217x有一个问题需要你这边帮忙解决一下,谢谢

对于DCDC电路上电瞬间,输出电压从0V开始上升,这个时候占空比开到100%,输出电压极具上升给DCDC输出端的电容充电,产生一个比较高的浪涌电流,电流的大小随电容的增大而增大,芯片规格书有提到有软启动功能,但是Vout是以大约25 mv/μs的斜率上升,按找芯片规格书推荐的22UF的容值,这个瞬间浪涌大约在550MA左右,但是因为我们后端的实际需求,当增加输出电容的时候,这个浪涌电流也会相应增大,最终导致瞬间浪涌电流会超过我的电感电流额定值,并且可能触发电流保护,输出电压波形在上升期间出现回钩。帮忙看下有什么办法减少浪涌电流?

  • Hi
    你讲到的是预偏执的时候,高边MOS打开而底边MOS不开,这个时候应该是一个恒流充电的过程,从第20页图30/31可以看到,有一段时间最大电流是保持接近恒定的,并且这个电流 不会特别大。
    你提到输出电压在上升过程中出现回钩,这个应该是负载瞬间启动造成的,相当于负载瞬间的动态调整。
    建议你增加外部软启动电路或者加一下前馈电容看一下效果?
    其次电感饱和电流不建议太小,如果容易margin,导致的饱和容易烧芯片。如果输出0.5A,建议选择1.35A以上的。
  • 你好,如上面所说,实际我的正常工作电流时非常小的,静态的时候只有150MA,目前电感是选用的800MA的贴片电感,但是我所遇到的问题就是上面你所说的在开机瞬间,输出电压爬升过程中对输出电容快速充电产生的浪涌电流比较高,输出电容22UF的时候大概是500多MA,但是我输出电容需要用到100UF甚至更大的时候,这样就会导致我的开机浪涌电流很大 超出电感应力,即使在空载的时候,开机瞬间电压爬升的这个过程中高边MOS打开,而底边MOS是不开的吧