This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61170做幻象电源的疑问



需要设计幻象电源,由于之前使用过61170所LCD的驱动,所以继续采用该芯片,原计划是5V输入,24左右V的输出,没选择输出48V是不想换芯片。

重新看手册时发现第20页,图22,整好为48V幻象电源的应用,但是手册里没有提到过可以输出48V,

请问该电路是否在芯片的功能设计之内?如果该方案可用,有没有手册中未提到的参数指标或者注意事项