Other Parts Discussed in Thread: LM26480, LM3881
现在需要对F28335和Cyclone IV E系列两块芯片及一些外围器件供电,需要的电压分别是3.3V 1.9V 2.5V 1.2V
之前一直使用独立的LDO供电,分别是LM1085-33, TLV1117-18, TLV1117-25和TLV1117-12,输入电压都是5V,用总线的形式把这些电源芯片连接起来供电。
现在有一个现象,就是系统运行的时突然断电,查到每个电源芯片的输出电压都是在4.2V~4.3V左右,断电重启后情况依旧。似乎把5V的输入端子重新插拔就好了。这种状态下似乎电流比较小,因为我的芯片都没有烧掉。这种现象似乎偶尔会冒出来,但是只要当时出现了,断电后现象会重现的
个人感觉像是LDO的电压调整失效了
另,对于我这种硬件,有没有什么比较好的供电方案推荐?我总觉得4个LDO不怎么靠谱