This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61220升压问题

各位专家好!

      我们最近在应用TI的芯片做一个穿戴式医疗设备,设备主体模块包括四个部分:1、电源部分(TPS61220);2、单片机(TI CC2640);3、AD芯片(TI ADS1191);4、FLASH存储(华邦)等。其中电源模块升压部分完全参考TPS61220的数据手册,电池采用CR2032纽扣电池,经过升压模块TPS61220升压到2.85V,供其他元器件使用。具体原理图参考下图。

     问题描述:在测试过程中发现,当给设备安装新电池或者电量比较足的电池时,设备能够正常工作,功耗也正常,电池输出端电流为1mA左右,一颗电池可以持续使用4天左右,与理论分析差不多。但是如果给设备安装已经使用过的电池,比如电压值2.8V,那么设备就无法启动,测量电池输出端电流非常大,100mA左右,电池两端电压为0.6V左右,TPS输出端为1.5V左右。把该旧电池正极直接接到TPS61220输出端Vout或者DVDD处,那么整个电路也能够正常工作,电流在1mA左右,说明电池本身还有较为充足的电量。

     现在我们非常困惑,不知道为什么旧电池无法正常启动设备。请各位专家帮忙分析指导,谢谢!

  • Hi
    新电池没有问题,就电池有问题。请问就电池的开路电压是多少?如果给它外部带载,例如2mA, 电压是否被拉低(可以用电阻来做验证)。
    我倾向是电池问题。电池电压低于0.7V,输出肯定无法正常升压,此时你需要注意电感可能已经饱和,导致电流非常大。(你可以选择更大饱和电流的电感,但是要注意芯片的输入电压必须保持在其可以正常工作的范围内)