This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

一块板子上有多路LM3409驱动电路

Other Parts Discussed in Thread: LM3409

一个板子上有多路LM3409驱动电路,通过PWM波进行输出控制,只接其中1路,工作正常,如果接2路及其以上,每一路都无法正常工作,无论PWM占空比多少,输出都很小。请教各位高手,是何处出了问题?

  • HI
    测试一下是否存在输入电压被下拉的可能,如果是,建议如下。
    主电源进去时走线宽一点,同时在输入处增加一个较大的电容,如100uF以上。
    到各自LM3409, 芯片也需要足够大的输入电容稳压。
  • 多谢您的回复!谢谢!我回去试一下!目前是这样的,在板子的主电源输入处,我放了330uf的电容,在LM3409的VIN处没有放大电容,您的意思是在每一个的LM3409的VIN处都放一个大电容,是吗?线宽应该是够的,80mil,接2路及其以上时,每一路的输出最大0.1A,单调每一路正常工作时,输出电流范围为0-2A。突然想到,会不会因为负载内阻太小而出现这个情况,负载内阻为0.1欧,会导致这个情况吗?
  • 你好,

    最好靠近每个芯片附近放一颗小电容,谢谢。