This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请假变压器过热问题



各位大神好:

 最近在参考TI的PMP5426原理图做个300K的电源,变压器自己绕,用的是PQ2625的磁芯,初级用0.41mm的漆包线,8根,次级用0.41mm漆包线,12根,匝数比为6:4,电桥测试电感为82uH,漏感100nH。输出正常,但是在满载10A输出时候变压器温度升到80°C,后来初级用12根漆包线,次级用15根漆包线,温度基本上也是80°C,这是什么情况?是用的线太粗了么?整流管和续流管VDS波形测试过,反向过冲不大于15V。36V输入,10A满载输出时测试纹波中有大于3MHz的高频杂波干扰。