This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

NB IOT 锂电池供电电源选择

Other Parts Discussed in Thread: TLV702

Dear:

    最近在做一个项目,使用3.7V锂电池供电(电压范围为2.5-4.2V),通讯使用NB IOT(工作电压3.1 -4.2,有时候电流会在200MA以上)。

    想选用一款LDO,暂时自己选的型号有TLV702  和TLLV733P 中转一下 ,此二款LDO看了效率都差不多。实际使用中那款会更好点。 比如电池供电降到3.5V,是否还如参考设计中能提供0.3A电流。 有无更好的建议。谢谢。

    

  • Hi
    选择LDO, LDO是降压型,如果你的ITO工作电压是3.1V, 算上Vdrop,电池的工作电压范围必须最低是3.2V左右。 LDO的效率就是输出除以输入,在参数相同的情况下,所有LDO的一样计算。如果ITO的输入电压更高,你就需要更高的电池工作电压
    如果你希望电池工作电压在2.5V~4.2V, 你需要选择升降压的DC/DC芯片,需要在电池电压较低的时候具备升压功能。