This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25606充电电流不稳定

Other Parts Discussed in Thread: BQ25606

各位好,

       目前我们在使用BQ25606的过程中,发现使用不同的充电器,25606的充电电流会出现不同程度的不稳定现在,只有用5V/2A的时候这个现象才会没那么明显,使用10W以上充电器时,会发现电流处于跳变状态,时有时无,像PWM波一样。是因为没有D+/D-通信造成的吗?片子内的保护机制起作用了才导致的这种结果吗?

       另外用2A充电时感觉电感和芯片发热有些严重,但也并未进入热保护状态,这正常吗?

       感谢!

  • Hi
    建议你首先确认你选择的功率电感饱和电流够不? 5V电压比较低,如果用更高的电压异常更加明显或更说明是电感问题,电压越高峰值电流越大,那么电感的饱和电流要求越大。 其次你提到5V/2A, 你还需要确认你设置的充电电流,功率上输入必须足够满足充电,否者会不稳定。
    对于芯片发烫,你需要确认Powerpad的散热设计,注意参考datsheet,特别是四层板,通过打孔扩张到中间GND层,利用其散热。