This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63060DSCR输出电压不稳定问题

我的输入电压在4.5V*5.5V之间,输出5V,负载电路峰值电流320mA,但是在实际使用中,发现输出电压很不稳可定,最大压降可达0.9V。然后我在输出端并接了两个1000uF的电容,并无明显改善。为找到原因,我使用稳压电源供电,发现输入电压在5.8V及以上时,输出压降很小,但是往下调节输入电压时,输出压降明显增大,请教各位大大,这个是什么原因造成的