This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24707A充电管理芯片 控制无输出现象咨询

Other Parts Discussed in Thread: BQ24707A, UCC27201, BQ24707

德州仪器技术支持工程师:

你好,我最近设计一款充电器,采用BQ24707A充电管理芯片方案,有些疑惑,请求帮助,谢谢!

设计原理图请见附件。

问题描述:

HIDRV和LODRV引脚只在上电后写入设置数据有短暂PWM波形后就没输出了,无法控制MOSFET进行输出。

每次上电后读取BQ24707A寄存器的值都是初始值,写入数据无法永久保存,必须每次上电都写入,不知是否正常?

电路调试过程:

由于输入电压比较宽(18-34V)超过了BQ24707A最大输入电压,所以使用在BQ24707A和N-MOSFET之间采用ucc27201驱动,BQ24707A单独9V供电;

输出接锂电池是2串的,8.4V;

I2C接口和单片机通信,读取写入数据都正常;

ACDET引脚为3V; >2.4V

ILIM引脚是0.76V; >105mV

REGN引脚为6V;

BTST引脚为3.4V;

ACOK  IFAULT CMPOUT引脚均为低电平

CDQ03R0_Charge.pdf