This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54329DDA有7%的芯片会出现啸叫声



啸叫出现的概率大概是14块板会出现1块,啸叫声会跟随电流大小出现变化,例如系统启动时电流出现波动,啸叫声的大小和频率也会波动;这啸叫声应该跟电感和电容无关,我尝试过把一块不啸叫的板跟一块啸叫的板相互交换了这颗IC,原来不啸叫的板就会出现啸叫声,就是说啸叫声会跟随这IC走。

把负载加到80%以上额定负载,啸叫声会响一点,但不会啸叫的芯片还是不会啸叫的现象。

电路分为5V输出和3V输出两种