This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA199A2在使用过程中为什么输出没变化?电路时按照数据手册典型电路连接的,采样电阻330毫欧



前端是AC(220V/50HZ)/DC(12V,2A)的隔离开关电源;

我现在的设计是DC12V,当单路超过0.6A,就要通过ADC告知单片机;

我理解的INA199的使用方式如下:

A),把采样电阻(SHUNT RES)串在供电电路当中,通过此电阻两端的分压来计算此路电流;

B), INA运放把采样电压放大,通过ADC给MCU;

C),  MCU根据设定的电流大小,再确定如何做出相应的响应;

是这样使用吗?谢谢