我的LM5116电路,之前发过一次问题,问的是高压带负载损坏IC的。现在遇到另外一个问题,我的电路是想14V输入到85V输入都能输出12V,输出2A。而实际输入30V时只能输出0.5A,高电压情况没测试。我怀疑是因为我的电流采样没走差分对,就把CSG割线了,结果割了线它还是短接到GND的,把芯片吹下来,单独测芯片和裸板子,CSG都没短接GND的,不知道为啥焊上去它就自动连接到GND了,把引脚翘起来,它还是连接到GND的。是不是芯片的其它引脚接了什么地方,会导致芯片内部把CSG自动拉到GND了?还是我的IC又损坏了,可是我上电,电路仍然可以输出12V,感觉IC又没坏。好奇怪,不理解。如果它自动接地了,再走差分对就没意义了....