This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28056:布线问题(Vin较高时PFC电路不启动)



项目信息:功率200W (240~300V 0.75A)

现在的问题时,当Vin(AC)在176~220V之间时开机,电路可以正常启动,而Vin(AC)在220V~264V之间时开机,电路却有时不能正常启动。

下图是电路图的一部分:

另一部分:

布线图:

调整C31(上图黄框里面)的GND接线后有所改善,但问题依然没有完全解决。

请问布线需要如何调整才能改善这个问题?