This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

电量计BQ34Z100G1的update status一直都是0x04。充满电静置的时候上位机一直显示有6ma的电流,静置两个小时VOK未清零,update status还是0x04,



电量计BQ34Z100G1的update status一直都是0x04。充满电静置的时候上位机一直显示有6ma的电流,静置两个小时VOK未清零,update status还是0x04,怎么解决?

  • 您好,请确保FC置位后充电器已断开,如果FC未置位的话,您需要检查一下器件设定以确保FC会置位。充满电后请静置两小时以上(有的化学体系可能需要静置5小时以上),再用合适的速率放电至截止电压,静置5小时。这时您应该能观察到update status从0x04变为0x05。重新充电并重复上述步骤,update status会更新到0x06。

    如果经过上述步骤问题依然存在的话,请提供一下您的详细配置,包括battery chemistry, max stack voltage, series cells数量, 外部分压电阻的值, current divider size 并上传您的gg.csv file.

    请问您的chemID是多少?是使用http://www.ti.com/tool/GPCCHEM 工具得到的吗?并检查一下IT是不是已经使能了?
  • 您的电流是否做过校正,先做一下校正看一下。