Other Parts Discussed in Thread: UCD9248
1) UCD9248一共有8个DPWM输出,是否DPWM-1A必定和DPWM-1B 频率相同?它们的相位有关系吗?DPWM-1A和DPWM-2A是否具有独立的频率?
2)产品手册第12页 “The UCD9248 contains four fusion power peripherals (FPP). Each FPP can be configured to regulated up to four DC/DC converter outputs.”这句话的意思是否是UCD9248有4个控制通道,每个控制通道最多可以带4个power stage?例如DPWM-1A和DPWM-1B是一个控制通道的输出,可以各带两个power stage,一共可以带4个.
我估计我的理解不对,是否可以画一个简图让我看一下这句话的确切含义?
3)产品手册第19页“The UCD9248 can control up to four rails, each of which can comprise a programmable number of power stages.”
我的理解是每个电源通道可以由若干个power stage构成。举个例子,在产品手册第9页的Figure 4 中,第一个rail就有8个power stages构成。这个理解是否正确?
谢谢。