This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

4.45V的充电电压IC

Other Parts Discussed in Thread: BQ24157, BQ25601

Dear All,

需要一款开关型充电IC。需求是:
1)充电电流1.5A,尽量非快充,快充的话多为I2C接口,会暂占用单片机的一些资源;
2)封装尽可能小,比如MSOP或者DFN封装,最好3*3mm以下;因为手电筒的体积很小;
3)可以在4.2V基础上正向调整满电电压(我们需要调到4.45V左右);这是一个二极管的形成压降;
4)频率尽量在600KHz以上,以便电感可以选用小封装的。
5)如果可以的话,尽量要非同步的,我们是用USB 5V充电,同步整流无法100%占空比,由于客户抬升了充电电压,会导致充电压差不足。
   像这一类的充电IC,很少有超过4.2V的充电电压的,TI这边有嘛?