This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100温度测量范围问题咨询

    规格书上说,内部和外部温度测量的AD为16位,测量范围为0-6553.5ºK

实际模拟测试时,使用外部温度测量,开路温度电阻显示为-39℃,短路温度电阻显示为123℃。

请问能否调整温度显示范围至少到-55~125℃或更高。(温度探头实际使用为103F3435,与规格书推荐的AT103参数很接近,给的参数表范围为-55~125℃)