This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请问我利用5V 800ma,给超级电容充电,再利用超级电容放电,输入给TPS63020,使其输出恒定电压,图片如下,有如下问题

Other Parts Discussed in Thread: TPS63020

 问题1:5V 800ma,要求只能充电一分钟,应该怎么给超级电容充电最快,效率最高,超级电容规格应该如何选择,电容是应该并联还是串联好?

问题2:我们有两个TPS63020模块,输入都是1.8-5.5V,输出一个是3.3V,一个是5V,现在超级电容放电给TPS63020,经过TPS63020的升降压,一个可以输出3.3V,一个5V,那么请问这两个模块,对电容放电效果一样吗?是否5V比3.3V放电快一点呢?

问题3:如何控制在给超级电容充电时,不会给TPS63020供电,超级电容供电断开时,自动通过超级电容给TPS63020供电呢?