This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5117输出电压被拉低



设计指标是输出20V,6A。输入电压在24V到30V之间。

在实际轻载时(使用舵机,舵机未带载),舵机转动,输出电压降至15V左右,刚启动时,最低可达5V,输出电压曲线不断跳动,直至完成打角。由于使用的是恒压源测试,恒压源上显示电流在0.4A以内。

原理图如下

不知道为什么电压会被拉低。