大家好,
我现在在设计TL431的反馈电路,根据TL431的datasheet,其Vka必须大于2.5V才能正常工作,但在我的电路中,不管怎么改各个电阻,Vka的值永远在2V上下,在Vka等于2V时TL431似乎会失去类似放大器的作用,在用环路分析仪测试补偿网络时显示补偿网络没有起一点作用,请问我该怎么设计才能把TL431的Vka拉到2.5V以上?我的反馈电路图如下图:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
大家好,
我现在在设计TL431的反馈电路,根据TL431的datasheet,其Vka必须大于2.5V才能正常工作,但在我的电路中,不管怎么改各个电阻,Vka的值永远在2V上下,在Vka等于2V时TL431似乎会失去类似放大器的作用,在用环路分析仪测试补偿网络时显示补偿网络没有起一点作用,请问我该怎么设计才能把TL431的Vka拉到2.5V以上?我的反馈电路图如下图:
文中提到了K极只能下降到Vref,这又回到了我的问题,我的KA电压一直处在2V
是这样的,最开始我的反馈环路在额定负载下能输出5V,然后开始用环路分析仪量测量波特图,发现无论怎么改补偿参数都无法改变波特图的形状,当时测得TL431的Vka一直处于2V的状态,然后在面包板上焊了下图电路并且手动改变右边的直流电阻值观察Vka发现它大于Vref大于2.5V时饱和2V,Vref低于2.5V时断路,因此得出了TL431像比较器一样工作因此补偿网络毫无作用的结论。
然后我看了前辈关于内部基准2.485V的提议,然后实际跑了上面那个电路和自己买来的电源后发现,Vref必须在2.485左右一个很小的区间内,TL431才会作为运放工作。我现在的想法是,不再直流跑反馈电路,改整个电路一起跑,测量采样和送回芯片comp端的电压慢慢进行调整,请问这样的试验方法可行吗?