This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3409HV调节频率问题

Other Parts Discussed in Thread: LM3409HV

LM3409HV,输入48V  输出28V  2.2A  用的MOS是AO4421,做了十多个样品。

大部分在频率400K的时候工作正常,其中一个用PWM调光微亮的时候工作正常,100%亮度马上烧MOS,怀疑是电感饱和

于是把之前测试OK的样品频率调高到600K,上电后MOS管烧了,为什么会这样,频率调高后通过电感的峰值电流不是应该降低吗