This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请大师过来帮忙解决。BOOST电路,TPS61030满载上电时无法启动



     电路见下面。BOOST  输入3V-3.65V   输出4V   2A。

     问题:

      Start-up current limit  为0.4 Isw  也即为1.6A。 我负载为2Ω,此时上电时,理想情况下输出端电压为3.2V,而实际上还有MOS管分压,电压低于输入电压很多,BOOST电路一直无法启动。

负载调整为4Ω时,也是无法启动。

示波器抓取输入、SW、输出端波形,都是平稳的电压波形。输出比输入低0.4V左右。

而空载时,先让芯片启动,再加上负载2欧姆,电路正常!

换了各种输入输出电容 电感,都不行。

请问如何解决????