This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq24133 快速充电时间TTC应该怎么设置?



按照手册上说说的,TTC时间达到以后会关闭充电。

我现在用的3串8并锂电池,容量27.4Ah。快速充电电流设置为2A。 27.4/2 =13.7 h  。

我设置这个TTC时间应该大于13.7h还是小于13.7h为好呢?

ps:我实际使用的是0.1uF 并联0.033uF 。 TTC时间为 133 *5.6  =12.4 h。  是略小于13.7h的。

感觉应该是要设置大于13.7h 。