This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于BQ77PL900内部NMOS需要电压



在上一个问题得到解答后,研读手册遇到一个小问题

在手册中有这么一句:The interrnal NMOS requires approximately 1.25V to 1.5V(depending on the value of external resistors selected)

不知道内部NMOS需要的电压和外部的电阻具体是什么关系。

希望能得到相关的解答或者解释。

  • 根据文档中的图表,可以把NMOS的DS与Ids分成两段即1v, 1mA到1.3V, 3.3mA作为一段,另一段是1.3V, 3.3mA到2V, 13mA作为一段,选择你想要的均衡电流, 在这个曲线上得到这个电流下对应的均衡电压,再根据均衡电流为0时的Vds电压,把这两个电压的差值除以均衡电流值,就可以得到Rext的值