This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54528

Other Parts Discussed in Thread: TPS54528

Hi TI工程师:

    我的客户使用TPS54528做12V转5V/2A应用,生产了50套,测试时发现有3PCS TPS54528 PIN SW和GND短路了。

    客户的生产完PCBA后会有两阶段测试,第一阶段半成品测试,第二阶段成品测试,差异在于成品比半成品多涂了一层防水胶。

    每一阶段测试又有两个部分,第一部分先做电气测试,电气测试阶段输入和输出都是通过连接器和外部设备连接,连接完好后再上电测试,输出5V接电子负载,模拟负载电流2A上升至5A,测试过程操作有带手套和静电手环。第二部分测试通讯是否正常,有专门的测试治具,将板子放在治具台上,通过顶针接触板子做测试,治具有小程序会显示测试是否通过。

    客户第一阶段的两部分测试都通过了,在第二阶段的电气测试也通过了,但在第二阶段的通讯测试发现3PCS通讯异常,确认是TPS54528不良导致,测试发现SW和GND短路。我们在产线现场做检查,发现电气测试部分操作应该是没有问题,但通讯测试的治具台没有设计的很好,板子摆在测试台上并没有完全固定住,有可能没摆好就会出现偏移,导致顶针接触板子时将5V和GND短接了。

    我们怀疑是治具测试时,顶针短接5V和GND导致TPS54528损坏,所以做了一些短路测试,上电前将输出5V和GND直接短接,然后再上电,TPS54528做了过流保护未损坏,也尝试了在5V正常输出时,直接对地短路,IC也做了过流保护未损坏。

    所以请问,综合上述的测试环境,什么情况下TPS54528会被损坏,导致SW和GND短路呢?