能解释一下Bit0,Bit1,Bit2的作用吗?
bq27426
Technical Reference 里面并没有提到。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请查看match ID的结果,里面有一项match的精度,是否在3%以内?
配置需要根据你电池的厂商给的手册配置gg。
Hi Eason
你的意思是没有获取匹配的CHEM ID?(CHEM ID是在TI官网上获取的)
只是学习时没有完全按获取的CHEM ID参数来设置,
比如:
1、获取CHEM ID的放电截止电压设置是2.5V,而已学习的放电截止电压设置是2.7V
另外:
充电截止需要3个条件:
1、During two consecutive periods of 40 seconds:
IRateAvg1 < Taper Rate and IRateAvg2 < Taper Rate
2、During the same periods: Accumulated change in capacity per 40-second period
3、Voltage() > Taper Voltage
现在只是明白第3点,能否解释一下第1、2点,
以上谢谢!
Hi Eason
按你说的方法问题已解决,谢谢!
另外,手册上描述 MCU只能配置三种固定的化学ID,我想写入其它的化学ID 比如2155,可是手册上并没有给出化学ID的 Subclass ID 与Offset,能否提供一下?
谢谢!