25V供电,VCC正常(比VIN小7.7V),反馈电阻R1为15K,R2为1.1K,输出为15-24V可调,Rt=300K。出现以下问题。
1、PGATE输出一直为VIN,但是输出却有电压(5V左右,调节出来的),但是没有驱动能力
2、此时的FB电压为4.13V,电路不工作。
PS:换了好几块芯片问题多种。。。很纠结,电路是按照WEBENCH给出的设计的,元件值都是给定的,然后MOS管也是用推荐的,之前第一块板子是可以调节电压,也有驱动能力,但是纹波比较大,看了一下开关频在30K左右,和设定的差别很大。