This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65983 Thunderbolt测试问题



1.,产品上电,将一个测试治具(test fixture)连接到产品上,将示波器连接到治具上抓取产品TBT3接口Vbus输出的电压及电流,将一个电子负载仪到治具上,再将一个PD 诱骗器(PD controller)连接到治具上。产品跟PD诱骗器通讯,产品输出5V,调节电子负载汲取3A电流。
       

2、调节电子负载仪设置成short状态,此时产品TBT接口输出的电压、电流,再调节电子负载仪移除short状态,产品可以恢复电压、电流输出。

 

3、调节PD诱骗器让产品输出9V,电子负载仪还是汲取3A电流。调节电子负载仪设置成short状态,此时产品TBT接口输出的电压、电流如附件“9V.png”所示。再调节电子负载仪移除short状态,产品输出的电压、电流无法恢复。

 

4、经过测试分析,发现这个样机的TPS65983的 C_CC1/C_CC2 两个PIN脚与GND短路,TPS65983损坏。

 

5、我们用在TPS95983 PP_HV channel上的DC-DC IC是 SY8204,这个IC自身有短路保护,我实际测试了这个IC,过流保护的特性与datasheet一样。

 

6、我用另外1pcs 样机模拟测试9V Vbus short protect测试,波形如下(用虚拟示波器抓取,信号有缩放,可供参考,电压需要放大10倍,即是一格为5V,时间一格为1s),黄色是电子负载仪端的正极(也可以看作是TPS65983的Vbus(H11/J10/J11/K11)),蓝色是TPS65983的PP_HV(A6/A7/A8/B7)。负载仪设置为short的瞬间,TPS65983先触发短路保护立即关闭PP_HV通道,所以输出的VBUS电压下降;由于TPS65983关闭了PP_HV通道,所以SY8204没有触发短路保护,可以看到下图蓝色的PP_HV PIN脚上的电压还是9V。然后TPS65983通过GPIO5将SY8204的输出电压改为5V。TPS65983每隔400ms左右就打开一下PP_HV通道(如 5V.png,9V.png 的波形),发现短路还是存在再关闭PP_HV通道。4.5秒后设置负载仪移除short,TPS65983恢复成5V@3A输出。

 

7、在我这边在这个样机上多次测试5V、9V的短路保护,都没有出现样机烧坏的现象,但在百佳泰那边测试,两台样机都是测试到9V Vubs short时将样机损坏。可能是我的测试仪器及测试手法与百佳泰的有差异。

 

8、请帮忙确认如下

    1)上述TPS65983的的行为是否正常?TPS65983自身是有过压保护、过流保护、短路保护的吧?

    2)请帮忙确认这款产品的TPS65983 FW(附件pjt档案)是否正确,是否是最新的FW,是否是适合这款产品的FW?

    3)请帮忙了解一下上百佳泰测试Vbus short protect 的手法是否正确?在这种情形下为什么会损坏TPS65983?