请问TPS40210的输出电压是多少?在TI官网上面的搜索中查到TPS40210的输出电压最大能达到260V,可是在datasheet里面没有查到?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
用TPS40210做有些复杂,不如使用LM5001,更加简洁迅速,但是需要做一些改动满足100V输出应用(因为LM5001的最高输出电压只支持到75V,所以通过串联MOSFET提高耐压等级来得到超过75V的输出电压)
在电感与芯片SW之间串联接入一只N沟道的MOSFET,耐压在60V即可,导通电流取1A就够了,然后MOSFET的S管脚与芯片的SW连接,MOSFET的G管脚与芯片的VCC连接,MOSFET的D管脚与电感的输出端连接,环路补偿用的参数可以使用LM5001的评估板参数即可,当然输出用的分压电阻阻值需要根据100V的输出来更改即可,附件中评估板的COMP对地管脚的二极管、RC使用于输出缓启动的,你的电压太高,这个电路有必要保持,否则对输出电容的冲击太大。