This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于EMB14228+EMB1499中TIDA-00817多路主动均衡方案能量来源问题请教。



已研究BMS一年多,在1A左右主动均衡时很多方案大都只体现其优势,但在项目要求2A3A或更高主动均衡电流时,体积庞大价格昂贵等劣势明显。只怪自己太愚钝近几个月才发现TI给的TIDA-00817方案,在价格体积性能等方面做的非常优秀,但在方案中有个问题如何也无法理解,以及更改方案时遇到的一个疑惑。

TIDA-00817是双向均衡方案吧,主动均衡时能量来源于外部隔离12V,这隔离12V由其它BMS Module产生的,这在主动均衡时还好理解,我用一DCDC隔离模块,输入为电池组电压,输出为隔离12V,然后经隔离变压器给某节电池充电;但在被动均衡时如何工作?单体电池的能量经隔离变压器反馈到隔离12V,然后再去哪里消耗或储备???

还有第二个问题,如果将主动均衡能量源由隔离12V改为本电池组,则遇到隔离的问题。EMB1499和EMB1428共地,即电池组负端,在隔离变压器T1原边驱动mos管的所有信号原本是和隔离12V共地的,隔离12V改为本电池组后,那驱动mos管的所有信号就和本电池组共地了,那隔离芯片U3  ISO7342就没有存在必要了,这样是否可以?

请教了,非常感谢。