This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24133充电 电流失控变大,SW占空比100%

hi all

我现在遇到的问题跟题主的问题是一样的,我预先设置的电流是2.5A,其中输入电压门限是13V,CELL pin float。上电后测量各管脚,REF 3.3电压是正常的,未接电池时,电感输出端的电压不是输出8.4V,指示灯闪烁。上电后,电池充电电流是1.7A,同时,指示灯常亮。测量SW脚,波形是16Mhz.掌控比很小。调节输入电压,到12.4V左右,充电电流急速升高(属于失控状态,到5A),测量SW脚发现,开关波行占空比会逐渐变小,知道变成一条直线,将电压减小,发现又可以恢复充电。这问题跟题主问题是一样。尝试更换更大电感,没有效果,更换了新的芯片也没有效果。

请问,

1.在没有接电池是,电感输出端的电压是否应该是8.4V,我的电路在没有接电池时输出是没有8.4V。电压跟电源输入电压略小。同时SW没有开关信号的波形,

2.接上电池后,SW波形会变成直线,这个是与设置参数有关系吗?

  • Hi
    功率电感主要是饱和电流足够,如果涉及2.5A, 饱和电流建议大于3.2A.
    没有接电池充电,见datasheet 9.3.15 Battery Detection描述,此时实际是给输出电容充电的一个过程,输出电压不会是8.4V.
    其次设置2.5A充电,异常到了5A, 应该早就过流保护了,建议确认一下sense电阻。
    电路可以参考datasheet,主要就是电池数量上的设置。