我使用TPS73733的时候,发现有时候OUT管脚输出电压不准(0.3V左右),FB/NR管脚电压也不对,只有1.15V(正常情况下1.2V),各位有什么解决办法么(重新上电后又可以)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我使用TPS73733的时候,发现有时候OUT管脚输出电压不准(0.3V左右),FB/NR管脚电压也不对,只有1.15V(正常情况下1.2V),各位有什么解决办法么(重新上电后又可以)
Hi :
能否具体说明一下:如输入电压,输出电压,以及负载。 需要知道知否是因为Vdrop或者负载造成的?
layout上要求输入输出电容尽量靠近芯片输入输出脚,采用低ESR陶瓷电容,以及分压电阻采用1%甚至更高精度,同时要注意散热设计等等。
我的输入电压是5V,使能脚是接的5V,电容之类的都比较靠近管脚,6脚(背部焊盘)接地良好,我的TPS73733不是可调输出,为固定输出3.3V