Other Parts Discussed in Thread: PGA281, PGA204, MSP430F5529
大家好,最近我正在使用TI公司的运放芯片PGA281、PGA204。测试过程中发现一些问题,我自己无法解答,麻烦各位解惑了。
ps: 本人学生一名,第一次使用PGA281和PGA204,关于两款芯片的使用方法,PGA281完全是按照数据手册的推荐电路,PGA204数据手册上的电路没看懂,参照了TI社区(此论坛)上面的电路。
我的主要目的是采集20-100uV级的低频信号(忽略为直流吧),这两款芯片是和老师商量之后决定的(老师说PGA操作超级简单,2222)。当初是我一个人设计电路的,(老师当时不在学校,出差),这几天电路焊接完成后与我所需不符,总述问题如下:
1.我把P1口短接,PGA281、PGA204增益全设为1,但是在PGA204输出端口测得电压4V左右(照理说应该是0V左右)。
2.我测试PGA281(PGA204因为layout原因,不便测试),我发现DC 12V的电源怎么变成6.x伏了?还有DC -12V怎么变成-17.x伏了?(我使用数字电源测试的)
电路图如下:
ps: PGA204的输出是Vref + Gain*(IN+ - IN-),按理说短接PGA281输入PGA204应该输出2.5V(两款芯片增益都设为1)。但是我现在不管怎样PGA204输出都是4V左右。
麻烦各位解答了。