使用bq24253作为电源,bq24253的输入端是USB,输入电压是5V,如果是接usb充电器,即使没有接电池,bq24253得到5V输入,被bq24253供电的PMIC也可以启动。但是如果usb线接到电脑上,即使也是5V输入给bq24253,被bq24253供电的PMIC就不能启动,除非是接上电池,此PMIC才能启动。请问这是什么原因?还望赐教,非常感谢!
更新
-- 型号之前写错,是bq24253。更正一下。谢谢TI的支持。后来调出原因,请见下面的回复
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
是用电脑上的USB给bq24250供电,电流应该是够的。因为板子插入电池,用电脑上的USB给bq24250供电,板子是可以起来的。但是只要不接电池,电脑上的USB给bq24250供电,板子就起不来。
调试完成了。我们用的是bq24253不是bq24250(之前同事发的有写错),带D+/D-的USB检测。插电脑的时候检测到USB2.0就直接限制了电流(没有接电池, 按Dead Battery算,100mA?),然后后面的电路就都起不来了。插充电器没有检测到USB2.0,就按预先设计的2A电流工作。后来设备的功耗控制的好一些,就不用电池供电也可以工作了,就把bq24253直接跳线短接了,后续的设计都把这部分删掉了。