This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5032低压无法启动

Other Parts Discussed in Thread: LM5032

我用LM5032芯片设计了一个反激变换器,输入电压为16-38V,输出为28V/0.5A和5V0.2A,28V过流保护为16V输入时1A保护。可是在16V输入下无法带载0.5A启动,实测0.1A负载依然无法启动,空载启动之后带载正常工作,这是什么原因?

  • Hi
    将电路传上来看一下? 输入电容多大? 测试一下带载启动,是否过流?
    另外SS电容适当加大一点看看?
    有可能是变压器设计不太好,或者是layout也有可能,建议逐步确认。
  • 输入有个6800uF的储能电容器 现在确认是启动瞬间过流保护,疑惑的是+5V输出启动瞬间没问题,+28V启动瞬间会过流
x 出现错误。请重试或与管理员联系。