按照手册推荐电路绘制电路,输入3.3V,输出±5V。
在断开负载,或者在±5V输出端分别加入51k负载电阻,TPS65133的静态工作电流达到25mA。
测试时,周边无其他电路,且测试两块PCB都是同样的问题。
请问,TPS65133的正常静态工作电流是多少?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
按照手册推荐电路绘制电路,输入3.3V,输出±5V。
在断开负载,或者在±5V输出端分别加入51k负载电阻,TPS65133的静态工作电流达到25mA。
测试时,周边无其他电路,且测试两块PCB都是同样的问题。
请问,TPS65133的正常静态工作电流是多少?
你可以参考一下我们的EVM板,IQ在10mA左右。25mA电流有些大,需要看一下你的测试方式是否有问题。
TPS65133 Evaluation Module (slvu940.pdf)
http://www.ti.com/litv/pdf/slvu940
首先感谢回复。
我在输出空载和51k负载下都进行了测试,静态电流在25mA左右。
EN脚拉低后,静态工作电流低于1mA。