This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC28700两路输出接负载的问题

Other Parts Discussed in Thread: UCC28700

用UCC28700设计了一个电源

输入 85-265

输出 5V /2A

24V/0.2A

发现如下问题

5v接0.4A负载,24接负载瞬间,5V电压变化比较大,能到500MV,然后恢复正常

5V接1A负载瞬间,电压能够降低到3V,然后升高到7V,然后恢复正常

这个原因可能是?