Other Parts Discussed in Thread: LM27762
第一次应用LM27762电源芯片,按照数据手册推荐电路配置的外围器件,输入电压5V至5.1V,设置输出±5V,问题:
1、在前两块电路板焊接调试时,不焊接电容C8,其他参数按照图示,正负端均有输出,只是低于5V,焊接C8负电压无输出,正电压拉低;
2、重新焊接3块电路调试时,还是按照步骤一同样操作,没有负电压输出,开始怀疑焊接问题,找专业焊接人员重新焊接后,问题同样在,最后尝试调节外围器件,将C7、C9、C10全部调整为1uF后,有输出,正电压4.8V左右,负电压4.3V左右(配置输出5V),但是还是不太稳定,有时上电启动没有负电压输出,且芯片有鸣叫。
3、哪位大侠以前如果用过方便的话恳求单聊(2363870039),急。