This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS3823 看门狗在插拔USB时触发RESET问题

Other Parts Discussed in Thread: TPS3823

 1.机器带电池工作,在电池低电工作的时候,插入或拔出USB,看TPS3823的RESET信号触发。

 2.机器在工作的时候,启动WFI,功耗增加,有时也会触TPS3823的RESET.

 VDD 3.3V 

 MR为高电平

WDI  一直有3.3V 高电平100ms, 低电平 100ms的信号输入,示波器测量过。

请问 WDI输入的脉冲是否正常?

这个可能是什么原因导致触发了RESET?

谢谢!

x 出现错误。请重试或与管理员联系。