Other Parts Discussed in Thread: TPS63031, TPS62160, TPS62147, TPS62170, TPS560200
要求输入2.8-20V左右的芯片,输出3.3V的电源芯片,请大家推荐一两款;
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
LM2578无法实现BUCK-Boost,也就是不能在2.8~20Vin下实现3.3Vout,因为这既需要升压也要同时可以降压,
你的这个电压范围单芯片不是很好实现,电压范围可以压缩一下吗
如果你是一节和三节锂电池,那么输入电压应该在3.7V~12.6V左右,单片机供电电流应该也比较小
可以看看那TPS62170(3~17Vin 0.5A),如果电流要求大的,可以TPS62160/TPS62147(3~17Vin 1A/2A)
如果你是两节或三节电池,那就可以降成本,可以选TPS560200 (4.5~17Vin 0.5A)或TPS56X201(4.5~17Vin 1~5A)