This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

3相PFC

Other Parts Discussed in Thread: POWERSUITE

使用powersuite设计三相vienna PFC时,当我在powersuite中gui界面配置参数时,直流vout(rms)设置为270v,交流vin(rms)设置为199v时,按确认键后,vout(rms)变成309v,这是为什么?

我的要求如下:

你好,我的技术要求如下:

交流输入电压范围110V AC,工作频率400Hz;

输出电压270V DC,纹波电压±10V以内;

三相功率因数均不小于96%,THD不大于5%;

输出功率不小于3KW,效率不小于90%

三相VIENNA拓扑结构能实现吗?

如果能,怎么设置powersuite中的参数