This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
UCC28610的VGG电压总是16V,VDD13V,感觉芯片没有起来,但是外部MOS管又很烫,搞不懂。求大神指点12
↑DRV驱动1
↑DRV驱动2
↑ VGG蓝色,VDD黄色
辅助绕组波形1↑
辅助绕组波形2↑
我重新调整了下PCB布局,现在管子不热了,可是电路还是感觉只起来一半,输出峰值能达到5V左右,然后迅速回落。波形如上
上面量的DRV的波形不对,这边重新上传一下
放大如下↓
首先谢谢您的解答,
反馈的波形也没问题,现在碰到一个问题,ZCD脚对地测电压波形的时候,一上电,UCC28610芯片就坏,已经坏了4块芯片了,我现在都不敢测这个管脚了,不知道怎么回事。