This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

两个基于UCC20189A的BoostApfc电源串联后作为正负电源使用的动态响应问题

Other Parts Discussed in Thread: UCC28019A

你好

因为项目需要,现在我需要制作一个正负电源,其指标为输出电压±140V,单路最大输出电流4A,单路电源最大功率560W,总正负电源功率600W,并与电网隔离。目前考虑的方案是使用220V转双线圈80V的变压器从市电取电,再经过基于UCC20189A的BoostApfc电路得到140V/4A/560W的电源,将两个电源串联起来得到±140V电源。但这个电源带的负载比较特殊,在某些情况下变化非常快,最快可以以接近5Hz的频率从负电源满载到正电源满载变化,即现在正电源输出4A满载,负电源接近空载,0.1s以后我就需要正电源从4A切到空载,而负电源从空载切到4A电流。

我想请问这样的方案有没有可行性,UCC28019A的动态响应速度能不能跟得上,这样串联起来会不会存在危险,亦或有其他的方案可供参考。之前考虑过电网220V整流后降压到140V后再串联的方案,我认为这个方案可以得到比较小的纹波,因为可以一直从高压侧得到功率。但是查询资料后发现560W的Buck电源大部分要用到谐振电路,这是我完全不熟悉的领域,所以不知道难度会有多大。除此之外,这两个方案又各有什么优劣呢?

若是UCC28019A的方案可用,我还有个问题需要咨询:我现在考虑使用一个800VA变压器,原边为220V,副边为两个隔离的80V,那么EMI滤波器是只需要在原边安装一个呢,还是需要在两个副边各安装一个。如果需要两个副边各安装一个,那么直接使用220V的EMI滤波器是否可行?