This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PSR 產品與設計建議 12V/36W



請協助建議以下規格的電源設計, 是否有適合的 PSR方案

Vin: 90Vac~264Vac

Vout: 12Vdc(+/- 5%) / 3A

Dynamic Load: 10%~100%  Load (Vout 11.4V~12.6V)